4/26/2016 11:00 AM | |
Joined: 3/17/2013 Last visit: 8/25/2024 Posts: 481 Rating: (43) |
Ok I meant Result of Logical Additon Vijay |
4/26/2016 11:03 PM |
|
Joined: 1/5/2015 Last visit: 2/26/2024 Posts: 108 Rating: (4) |
Hi, Althou everything has been made clear by the experts one might want to google Bitwise operation in programming! There are also some additional information in wikipedia. BR |
4/27/2016 5:02 AM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello My favourite application ( and the one I use most often ) of OR WORD and AND WORD operation is to evaluate +ve or -ve edge of individual bits in a word. This way you can evaluate 16 rising / falling edges with a fraction of the Program code than what you would otherwise require. This is very useful for example to set an Alarm hooter on every new alarm. Here is a FAQ on how to do Edge evaluation Word-wise : Edge evaluation word by word Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
Follow us on