3/14/2024 7:51 PM | |
Joined: 9/9/2015 Last visit: 6/24/2024 Posts: 727 Rating: (273) |
It seems that your os client graphics files might have a graphics script problem. And seem like you have other os client that is having no issue. let me name them OSC_Bad and OSC_Good. I will do this to double check 1. backup the OSC_Bad folder (since this is the same with your ES, you may skip this if you want) 2. look for the OSC_Good that is being used by operator , which is healthy, copy the gracs files, and paste over to your OSC_Bad. (only GraCS) folder. 3. activate the OSC_Bad and check whether the same issue happened again. 4. if yes, deactivate it, and compare the rest of the files, ensure they are all the same. If the folders are the same, probably there are some windows settings/PCS 7 configurations having issues. Hope this is helpful. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on