2/8/2018 6:59 AM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating: (4) |
Hello Ahmed, It seems that wincc explorer is open on this machine and it does not have the OS engineering license. In case you are using this machine only for the OS runtime then you need to configure the Wincc autostart as described in the below link. in that case you need not to open the wincc explorer to run the OS runtime. https://support.industry.siemens.com/cs/ww/en/view/23061262
Best regards, nkr |
Last edited by: Jen_Moderator at: 2/8/2018 10:08:13 AMOptimized link. |
|
2/9/2018 7:36 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Ahmend, every time you use the Runtime, whatever OS or ES to make tests, you should have a license for the runtime. So you can buy a license for the ES, testing your system on the OS or started the OS simulation with SIMATIC Manager > Options > Start OS Simulation. Here some Links that should be useful: Best regards, |
Last edited by: Heisenberg2 at: 2/9/2018 7:37:58 AM |
|
2/9/2018 9:40 AM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi Ahmed, For the ES, you basically need the following license of type: 6ES7658-5AX28-0YA5: SIMATIC PCS 7, SOFTWARE, AS/OS ENGINEERING V8.2 FLOATING LICENSE FOR 1 USER E-SW, WITHOUT SW AND DOCU. LICENSE KEY ON USB STICK, CLASS A, 5 LANGUAGES (G, E, F, I, S), EXECUTABLE UNDER WIN7ULT/SERVER 2008 R2/ SERVER 2012 R2 REFERENCE-HW: PCS 7 IPC BUNDLE This license has AS and OS engineering license which means unlimited access to AS and OS engineering so you can edit WinCC with no problems (unless you are using additional packages which require a separate license. When you want to use your ES as Single Station -> ES + OS runtime, you will need the following license: 6ES7651-5AA28-0YA0: SIMATIC PCS 7, SOFTWARE, ES SINGLE STATION V8.2 (AS/OS: PO 250), SINGLE LICENSE F.1 INSTALLATION R-SW, W/O SW AND DOCUMENTATION, LICENSE KEY ON USB STICK, CLASS A, 5 LANGUAGES (G, E, F, I, S), EXECUTABLE UNDER WIN7ULT/SERVER 2008 R2/ SERVER 2012 R2 REFERENCE-HW: PCS 7 IPC BUNDLE |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on