2/2/2010 4:46 PM | |
Posts: 183 Rating: (8) |
Hello Plan B; Did you make the migration version by version? i mean: A) V6.0->V6.1 B) V6.1->V7.0 C) V7.0->V7.1 |
2/2/2010 5:27 PM | |
Posts: 5 Rating: (0) |
Njet, from V6.0 to V7.1 |
2/2/2010 5:40 PM | |
Posts: 183 Rating: (8) |
Hello plan B; Did you make the migration in a PC, where earlier versions of PCS7 were installed? |
2/3/2010 8:31 AM | |
Posts: 5 Rating: (0) |
No is is on a brand new IPC preinstalled |
2/3/2010 8:31 AM | |
Posts: 5 Rating: (0) |
No it is on a brand new IPC preinstalled |
2/5/2010 9:14 AM | |
Posts: 183 Rating: (8) |
How did you make the migration? |
2/5/2010 10:21 AM | |
Posts: 5 Rating: (0) |
Following the guideline for upgrading from 6.x to7.1 with update of the lib. Everthing went well until running the OS-project-editor |
2/5/2010 12:59 PM | |
Posts: 183 Rating: (8) |
Hello; Did you try execute OS project editor in original project version 6.x and then migrate? |
2/5/2010 2:27 PM | |
Joined: 4/5/2006 Last visit: 12/12/2024 Posts: 917 Rating: (63) |
Hi Plan B , did you already lookedfollowinf link? What can be the cause of the message "HResult Error" in conjunction with WinCC? hope can help regards |
Follow us on