9/20/2012 12:04 PM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, I suggest to place a diode between output and load to prevent reversed current to output transistor. All cards with redundant capability have build in Diode for that reason. Relais cards, don't care about that at all. Regards, Marcjan AttachmentDO-redundant.pdf (31 Downloads) |
Last edited by: Marcjan at: 9/20/2012 12:27 PMAttached example Problem solved? |
|
9/20/2012 12:48 PM | |
Posts: 123 Rating:
|
Thank you. I will consider it.
|
10/5/2012 3:40 PM | |
Posts: 123 Rating:
|
Price is just one of the aspect. The other is using standard module. I want to use:
Interface module - UMK 45-DO/LA/SIM 8 - 2968195 This one fit perfectly with a standard io module (not safe/ no relay), if I connect this with a ribbon cable to the interface card(System connectors - FLKM 14-PA-S300 - 2299770), then it's not possible to build a diode inbetween. I have tested the connection as I described here, it work. But I'm not sure if I can trust this behaviour. |
Last edited by: Bofely at: 10/5/2012 3:45 PM |
|
Follow us on