7/10/2020 10:32 AM | |
Joined: 5/23/2016 Last visit: 11/15/2023 Posts: 63 Rating: (10) |
Hi Duris! Thanks again for helping out In the attatchment you will find the screenshots of the settings. I've checked the device name once again and it was ok. I've assigned it Again and it checks-out the second time asswell. But still no data coming from the PAC3200... Status LEDs of the CP and CPU are only the SF, this is due to a read/write error in the program we are already aware of. Diagnostic events had nothing that could lead to the PAC3200. See the attatchment. We also have a PAC3200 over profibus (PAC3200_voorna) wich you will see in the DB, this one works perfectly fine. Hope you can find something in the settings! AttachmentScreenshots.zip (93 Downloads) |
Best Regards, |
|
Follow us on