7/12/2023 4:14 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986)
|
if you mean Powertag Licences then no additonal licence need |
7/19/2023 11:55 AM | |
Joined: 2/17/2020 Last visit: 5/31/2024 Posts: 1008 Rating: (177) |
Hi, As detailed in the manual below, that number is a hardware limitation of the panel model used: Comfort Manual - Scope of functions with WincC - Tags Unfortunately, despite the fact that TIA Portal (programming software) allows these limits to be exceeded, these are hardware limits for which the panel has been tested and, if they are exceeded, the correct operation of the equipment could not be guaranteed. Also, no additional licenses can expand this limit, as it is hardware related. |
A rating will be well appreciated. |
|
Follow us on