12/4/2020 7:19 PM | |
Posts: 25 Rating:
|
Slam shoma movagh shodid/ lotfan ba man dar sorate emkan tamas begirid. hamed.[snip] ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/07/2020 08:25:16New subject after splitting; E-mail deleted |
|
12/6/2020 11:37 AM | |
Posts: 25 Rating:
|
hi i have similar problem i need win ce 5 for reboot the hmi because i have not backup of project . i dont want to reset factory becuse i think that will clear the program . can you help me plz. [snip] ... |
Last edited by: CS Moderator at: 12/07/2020 08:26:55E-mail deleted |
|
12/6/2020 11:39 AM | |
Posts: 25 Rating:
|
?hi could you repair your panel mp377 |
12/7/2020 11:00 AM | |
Posts: 25 Rating:
|
hi dear i have similr problem how i can ask you thank you my mail is... [snip] |
Last edited by: The Helping Hand at: 12/07/2020 16:50:02Removed personal data - please use personal messages. |
|
12/8/2020 7:41 PM | |
Joined: 9/27/2006 Last visit: 7/22/2024 Posts: 12270 Rating:
|
Hello Tenoch; The "correct" NIC is the Network Interface Card that is installed on your programming PC, or one of them dedicated to the communications between the PC and the PLC in case there are more than one to choose from. Have a look at the following document for hint on setting up the PG/PC interface properly:: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible? https://support.industry.siemens.com/cs/ww/en/view/11870489 Hope this helps, Daniel Chartier |
10/11/2022 2:43 PM | |
Joined: 6/12/2016 Last visit: 7/10/2024 Posts: 3 Rating:
|
Hi, this week, I had this problem. There is a standard solution on this site: In the attached files, there is another guide with the same steps. But, to resolve this problem, You must review first, the next: 1.- Test the IP configuration of your adapter with another PC, laptop, Logo PLC, etc. to have the complete security of your good ethernet configuration. In my case, my virtual machine had a good configuration but my native does not. I had to disable my windows firewall. 2.-Complete the steps with the Siemens Standard Guide. 3.-It doesn't matter the IP of the HMI(because it doesn't have any image), the most important is the configuration in step 1. In addition, there is a suggestion to confirm the HMI device, in OP properties, but it's not necessary, the factory reset will start without problems. I hope it helps you. Attachment19701610_wincc_flexible_e.pdf (514 Downloads) |
Last edited by: Jen_Moderator at: 10/12/2022 08:03:50Link optimized. |
|
Follow us on