Industry Online Support
Technical Forum
11/6/2008 8:18 AM | |
Posts: 37 Rating:
|
Hello friends, I am using RedundantET200M, DPV1,12I/Oas slaveand CP5613A2 cards as master. As per the manual, i havedone a particular set of parameter assignment to ET200M. Now whenever, a module is plugged out and reinserted, the diagnostics do get updated but at the same time mastership switchover occursbetween the IMs. Which means that, the communication is stopped for a fraction of second and mastership gets exchanged between the 2 IMs. Please tell me is this an issue of ET200M 153-2,DPV1,12I/O or i need to give some fixed set of parameter data. This problem is not faced with previous versions of ET200M. I am attaching along the set of parameter assignment i have done for ET200M,DPV1,12I/O. Attachmentsnapshots.zip (186 Downloads) |
11/26/2008 2:53 PM | |
Posts: 5822 Rating:
|
Hello, do you run the ET 200M in redundant mode? This is not absolutely clear form the information you gave to us. Best regards J_Bell |
11/27/2008 4:47 AM | |
Posts: 37 Rating:
|
Yes, we run this ET200M in redundant mode. |
Follow us on