4/6/2020 10:59 AM | |
Posts: 36 Rating:
|
Hi! I have the same parameter problem. I use ET 200SP CPU 1512SP F-1 PN in a TIAPortal v15.1. I only wanted to connect to the PLC and write and test some sample projects. But after I added the PLC + moduls an error occured, the DQ modules show a parameter error (flashing red LED). The PLC error LED is flashing as well. Here is some photo of the project and the set up. /I am really new in 1500 models, only used 1214 before. So I am not experienced in configurating these./ Thank you! hajleh12 ------------------------------------------------------------------------------------------ AttachmentS7-1500 ET 200SP.zip (158 Downloads) |
Last edited by: hajleh12 at: 04/06/2020 11:01:00Last edited by: Jen_Moderator at: 04/06/2020 13:52:53New subject after splitting |
|
4/6/2020 12:16 PM | |
Posts: 36 Rating:
|
Okay, here it is. Regard, Lehel |
4/6/2020 12:47 PM | |
Posts: 36 Rating:
|
Yes, the server module is there at slot 10 and working. (not showing any error msgs) Attached the pictures. Regards, Lehel AttachmentServer_Module.zip (170 Downloads) |
4/6/2020 1:23 PM | |
Posts: 36 Rating:
|
Hello Hati! Here are the errors what I got. (3 errors) Regards, Lehel AttachmentDQ_diagstat.zip (153 Downloads) |
4/6/2020 1:39 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
have you checked the baseunitis? the message say that you mounted a different baseunit color. |
Follow us on