2/7/2024 3:59 PM | |
Joined: 2/12/2019 Last visit: 5/3/2024 Posts: 10 Rating: (1) |
Hi, Could anyone please assist, i am wanting to read the current parameter set type that has been written to the PLC and display this so the operator can see what parameter is in use. i have used the standard parameter set control. i have also created a button to read the parameter set name from the set type ID is there anyway of read the set type ID currently in use? TIA V18 update 3, device is a MTP1500 unified comfort panel. Many thanks in advance. AttachmentParameterSet.zip (105 Downloads) |
Follow us on