6/16/2021 8:43 AM | |
Joined: 3/3/2021 Last visit: 10/2/2024 Posts: 271 Rating: (33) |
Hello Tom, I would consider this as a Bug in the Software, maybe the Siemens Support can help you. Best Regards, Fred |
6/16/2021 10:36 AM | |
Joined: 2/16/2021 Last visit: 9/7/2022 Posts: 5 Rating: (1) |
I think it's correct. I also first tried to use the "Parameter Set ID" and "Job ID" to retrieve current data from the parameter set control. However, they are control tags. The "Parameter Set ID" tag should be set by the user to the ID of an existing parameter set. The "Job ID" tag is also set by the user to decide the action, i.e. uploading, downloading or deleting. See chapter "11.2.6 Transferring and deleting parameter sets automatically" in the manual. . |
5/4/2022 5:54 PM | |
Joined: 1/15/2016 Last visit: 6/27/2024 Posts: 2 Rating: (0) |
I found the same bug on Unified V17. Is there any workaround, so far ?! Thanks. |
6/2/2022 11:55 AM | |
Joined: 4/8/2016 Last visit: 5/6/2024 Posts: 14 Rating: (0) |
Hello, look here: This is a script solution. m_i_c |
7/1/2023 1:07 PM | |
Joined: 8/15/2022 Last visit: 4/25/2024 Posts: 9 Rating: (2) |
Hi,Professor.Can anyone solve this issue?.I Still Get Return 0 too. |
8/28/2024 11:28 AM |
|
Joined: 5/11/2022 Last visit: 9/5/2024 Posts: 1 Rating: (0) |
Any simple works solution |
Follow us on