Industry Online Support
Technical Forum
6/5/2012 9:25 AM | |
Posts: 9 Rating: (1) |
Thank you for your fast reply. I do use the DIS datatype. For mode 1 it works well. First I get the DWORD out in mode 0 to see which other modes are supported. Then I switch to mode 1 and get out the diag information. It works well. Just as in the manual. But then I switch to mode 2 and I get the error code 16#8081 as RetVal. This means that in the actual mode the parameter at output DIAG is not supported. As you can see in the screenshot of the watchlist the variable modi shows that mode 0-2 are supported. You can also see that in mode 1 I get the right information. And you see the RetVal_mode2 that is 16#8081. I hope you have an idea about what is wrong. Siemens wasn't able to help me yet. Thnak you. Andi Attachmentscreenshots.zip (249 Downloads) |
Follow us on