2/23/2015 9:25 AM | |
Joined: 11/29/2011 Last visit: 5/3/2024 Posts: 1357 Rating: (229) |
Hi, Tricky question. The only way I can think of is running using Wincc for that. Have a look at WinCC V7.2: Tools (SmartTools, User Archive, interfaces) under chapter "1.4.5.3 Integrating header files and DLLs". You could than access your data you need to write it to a TAG. Not a very good solution, but the only one I can think of. |
- What you read here, please check with manuals and your requirements. |
|
11/2/2015 2:30 PM | |
Joined: 8/15/2011 Last visit: 7/27/2022 Posts: 143 Rating: (12) |
hello, here SIMATIC ODK 1500S Examples https://support.industry.siemens.com/cs/de/en/view/106192387 |
8/10/2018 5:38 AM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Try this link: SIMATIC ODK 1500S SMX driver Using the SIMATIC ODK 1500S SMX Driver, custom user applications written in high-level programming language can exchange data with the PLC program running on the SIMATIC 1500S. A Shared Memory is created, which can be accessed by the PLC and the user application. Yu-wen |
Follow us on