6/14/2016 4:16 PM | |
Posts: 200 Rating: (6) |
Hi William i am with you and appreciate all the help given. I have had a good go of the project and have moved it on a bit further but as all ways have hit the wall and cant seem to work it out. I have added the program to the post. F1 is the main login and when using the password: ashline1 it then enters page 2 Functions. I can then use the buttons as per request. F8 is then used for access to screen 3 password: ashman01 this seems to work and the buttons within the screen to F5 is then used to return to the Functions screen. this all works fine until i have to return the 3 screen when it then uses the password: ashline1 so for some reason it changes the password. also i seem to have the issue again with the auto logoff which is totally bugging me. i do have a program that is V5 which works fine with the logging out automatically the problem has only come about by adding the 3rd page. Thanks for looking Andrew AttachmentMESSAGES_V6.zip (121 Downloads) |
Follow us on