Industry Online Support
Technical Forum
12/5/2014 2:39 PM | |
Joined: 11/23/2011 Last visit: 6/25/2024 Posts: 202 Rating:
|
Hello Zebulon59, why don't you upgrade first to the new LSC version V8? When you already have an older LOGO!Soft Comfort Version you can do this for free. Here is the link: Demo software , upgrades/updates, drivers Choose the right version of the upgrade-file depending on your operating system. Here you can see in two FAQs how you can upgrade manually or automatically through the software: With LOGO!Soft Comfort how do you make an upgrade, update or extension via the Update Center? How do you install a downloaded upgrade for LOGO!Soft Comfort with or without installed LOGO! software? In the FAQs the upgrading procedure is explained for upgrade to V7.1 but upgrade procedure to V8 is the same. With LSC V8 you can also use LOGO! 0BA5, so don't be afraid. Hope that maybe with an upgrade to V8 you can download and upload the programs in both directions without problems. When your problem still exists just inform us. Greetings, KM_AS |
12/5/2014 3:57 PM | |
Posts: 4 Rating:
|
Hi, upgrade to V8 did'nt solve the problem. However, V8 checks the communication to the LOGO prior to uploading, and says OK, but then the same problems occur. I attach screenshots, maybe this is of help for further ananlysis. Many thanks for your efforts! Zebulon59 AttachmentScreens.zip (225 Downloads) |
12/5/2014 10:46 PM | |
Posts: 5225 Rating:
|
Hi. I have only one thought: Is there any memory modules connected onto the base unit? w |
12/6/2014 12:10 PM | |
Posts: 5225 Rating:
|
Hi. I am sorry to hear about your problems. It does not seem as though us LOGO users are of much help to you. Have you asked Siemens for help? Support Request As my very last thought.. there was some problems by some about the use of USB3 ports. That is unluckily all I know. w |
Follow us on