2/10/2015 2:48 PM | |
Posts: 6 Rating:
|
i have a simatic manager v 5.5 but hen i connect the pc adapter it give me a message : "unknown device" .... if i updated my HW .... will it work ?? |
2/10/2015 3:01 PM | |
Joined: 5/12/2006 Last visit: 8/5/2024 Posts: 22334 Rating:
|
what do you mean with Update the HW? A new Adapter? |
2/12/2015 9:51 AM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating:
|
Hello, Updating HW catalog will not help. It helps only if you would like to download a new module which is not exist in the catalog of HW config. Please tell us what is your version of MS Windows and which SP? or check yourself the comptabity from this tool. And also see this thread "USB PC Adapter not installed with Step7 V5.5" specially the following reply:
Hope this helps. |
Ayman Elotaify |
|
Follow us on