1/8/2014 7:39 AM | |
Posts: 10 Rating:
|
Happy new yr guyz I am having issues with PC adapter MPI for TIA Portal V12. In the On line access tab, I cant find the PC adapter MPI. Please see the attached picture. I am having Step& Simatic Manager installed in the same PC. I can access the PC adapter MPI and can communicate with PLC. But this is not possible with TIA. I tried re-installing the software, but then also I faced the same issue. Please advise. AttachmentC:\Users\1007687\Desktop\Zipho\pic12.pdf (615 Downloads) |
1/10/2014 7:58 AM | |
Posts: 10 Rating:
|
1. The PC adapter I am using is with USB. I am also having PC adapter USB A2. (See picture:MPI.PNG)2. My windows Version is Windows 7 Ultimate- 32 Bit.In the online access (Check picture: ON line access-No MPI.PNG), I cant see any of my MPI drivers.When I tried to go online, I cant access to any of my other drivers installed. I could see only Teleservise (See picture-online.PNG).I am having Simatic manage 5.5 on this same system. I dont have any issues with that. Previously I was having TIA V11 working on this system without any issues. Recently I uninstalled TIA V11 and installed TIA V12. I tried installing 3 times to solve this issue. Still I am having the same problem. AttachmentC:\Users\1007687\Desktop\Zipho\MPI\Full page photo4.pdf (397 Downloads) |
1/10/2014 10:16 AM | |
Joined: 9/23/2005 Last visit: 3/24/2023 Posts: 4180 Rating:
|
Hi, wich version of V12 do you have? V12 SP1 upd3? |
Denilson Pegaia |
|
7/14/2014 12:31 PM | |
Posts: 2 Rating:
|
I'm having the same problem as the others, I'm using TIA PORTAL V12 without updates, help me please. |
12/2/2014 10:47 AM | |
Joined: 9/1/2005 Last visit: 3/23/2023 Posts: 4099 Rating:
|
follow up question published byjgutierrezis split to a seperate thread with the subject PC Adapter v5.1 (6ES7 972-0CA23-0XA0) for TIA Portal V13. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on