6/12/2020 10:57 PM | |
Joined: 9/27/2006 Last visit: 5/23/2024 Posts: 12257 Rating: (2668) |
Hello Mani; My first reaction would be that you could easily use ET 200M stations, with IM 153-2 interface modles for Profibus-DP, or IM 153-4 for Profinet,and S7-300 I/O modules to add you extension I/Os. This document can give you information on PCS 7 and extra I/O modules: Configuration of Redundant I/O Modules in SIMATIC PCS 7 https://support.industry.siemens.com/cs/ww/en/view/28430682 If your S7-414-4H is mounted as a redundant pair, you would use redundant ET 200M I/O stations, which requires 2 IM 153-2 per station (with IM/IM bus module), S7-300 I/O modules installed in their own BM/BM active bus modules (to create an active busplane that allows redundancy over Ptrofibus).. See the attached screenshot below. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/12/2020 23:00:34Last edited by: dchartier at: 06/12/2020 23:27:33 |
|
This contribution was helpful to1 thankful Users |
Follow us on