6/18/2013 3:19 PM | |
Posts: 836 Rating:
|
Which PCS 7 are you using? |
6/19/2013 7:44 AM | |
Joined: 7/6/2009 Last visit: 6/1/2022 Posts: 100 Rating:
|
ThanksSilent Bob, After Compilation, of the tags have been tranfered to TCP/IP Connection and i set it to PLCSIM TCP/IP , But , When i startWinCC Explorer > Tools > Status of Driver Connections , The status driver wasn't activated in the sub-menue ---- Se attached PIC-1 WHen I start the OS Simulation , it seams that the connection is OK but the same alarm message displayed TERMINAL ADAPTER DISCONNECTED ---------- See Attached PIC-2 Downloading PC station also Failed ------------- See attached PIC-3
AttachmentPIC.zip (370 Downloads) |
Walid Elshazly |
|
12/2/2015 8:41 PM | |
Posts: 163 Rating:
|
hello, I am facing the same issue. Any help guys ? |
Follow us on