6/1/2024 2:35 AM | |
Joined: 7/20/2015 Last visit: 6/22/2024 Posts: 154 Rating: (27) |
Dear All Block: - MotL Software; - PCS7 v9.1 I am not able to see motor running indication in local mode. I have put 1 in Local setting, And i got local selection feedback from field. I am not giving any output command in local mode. Only just want to see run indication. When the run feedback came from field, block icon is showing status error and MotL block showing Group error, How can i resolve this issue, to see run indication on MotL block icon. Thanks & regards Sandeep Bakoliya AttachmentMotL.pdf (17 Downloads) |
Regards |
|
Follow us on