8/30/2023 7:19 AM | |
Joined: 9/9/2015 Last visit: 7/29/2024 Posts: 727 Rating:
|
Hi all, I would like to share a workaround on PCS 7 V9.1 SP2 WinCC Runtime Workaround. Error Message Occurred during WinCC V7.5 SP2 Runtime Installation: xxx - System Error "The code execution cannot proceed because xxx was not found. Reinstalling the program may fix this problem." xxx = ACE60_x64.dll SCSDiscoveryX.dll CCCAGeneral.DLL CCAppHealthCheck.dll Solution: [NOT VALID , PLEASE READ THE BOTTOM THREAD] 1. Continue to proceed the installation till the end 2. Restart the station 3. Install the PCS 7 V9.1 SP2 again 4. Select User-defined package 5. Select WinCC Runtime 6. Install again and complete successfully. 7. Install update collection if required. Similar solution found here by eraabid. |
Last edited by: JazTai at: 08/30/2023 07:24:05Last edited by: JazTai at: 09/26/2023 20:09:13Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
2 thankful Users |
9/26/2023 8:05 PM | |
Joined: 9/9/2015 Last visit: 7/29/2024 Posts: 727 Rating:
|
This specific case was found during migration from PCS 7 V9.0 SP3 (IPC647D/IPC847D, Windows Server 2016/ Windows 10 LTSB 2015) to PCS 7 V9.1 SP2 UC02 (IPC647D/IPC847D, Windows Server 2019/Windows 10 LTSC 2019). When I used user defined method to install WinCC, the error disappeared , however, SQL 2017 was not installed by default , causing Simatic Manager unable to open OS project or create OS object normally. We were using “Microsoft Windows 10 IoT Enterprise 2019 LTSC 64-bit for SIMATIC IPC647D/IPC847D ( 6ES7650-4MB00-1UA0)” to restore windows image. The root cause is because when we restore the image, we chose "restore windows partition only" instead of "Reset partition and start everything from fresh". After we reset the partition and reinstall PCS 7 V9.1 SP2, this error was gone and SQL installed automatically as usual. An update of the solution above. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
9/26/2023 8:08 PM | |
Joined: 9/9/2015 Last visit: 7/29/2024 Posts: 727 Rating:
|
I believe you are saying PCS 7 V9.1 SP2 installation media. We used the extraction method (PCS_7_V9120.exe) , downloaded from Automation License Manager through Online software delivery. I did not face issue on this. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on