10/4/2016 4:37 PM | |
Posts: 46 Rating: (0) |
I deleted the DBs but now the problem exists all the time on DB2575 (POOL DB). the error remains and I am not able to download, help is appreciated, thanks, ElieR |
10/4/2016 6:07 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hello, Go to CFC-->Options-->Block types and clean up blocks from the cfc charts as well as the blocks folder via button: Clean up. Do a full compile and try a download change. A full compile means also a download to the OS. |
Last edited by: Oreca at: 10/4/2016 6:09:46 PMIf I could help you, you can use the RATE button. Thank you. |
|
10/5/2016 11:18 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, I think it was wrong to delete those DB's... What you can try (not sure if it works but if it does, you can give me a kiss), is to go to CFC chart->Chart Reference Data and go to View->S7 Resource Allocation. Find the DB under tab: "S7 resource" and see which configured object references that DB. Go to the CFC chart by right clicking on the object-> Go to point of use. Now insert the same object. For instance, if this is a MotL block, insert a new MotL block, drag all interconnections to the new block, create a temporary name for the object. Delete the "original" object and compile the program (full compile preferred). Then try to download your changes. Hope this works, otherwise, I think you have to do a full download, meaning the plant is shutdown... |
If I could help you, you can use the RATE button. Thank you. |
|
10/5/2016 12:12 PM | |
Posts: 46 Rating: (0) |
Hello, I have attached the status of the resources allocation, the CFC blocks and the download errors. please let me know what you think, Regards, ElieR AttachmentStatus.zip (73 Downloads) |
10/5/2016 12:42 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi ElieR, Well good that you can go online now. Nevermind the kiss I would be happier with a rating instead . I think you last option is to delete those Timer_P's and make sure you can go online again. Then, select the multiproject and then File->Save as, option: "With reorganization (slow)" checked. Then afterwards, add the timer_p and try again.. If not...I have to check myself if I can produce the error and try to solve it... Maybe your only option is to download in stop mode. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on