2/7/2016 12:16 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
I would like to get an example project where PCS7 version 8.1 SP1, With Indl Lib Ver 8.1 is used with S7319 CPU Standalone System. We need to create a system which is using the said hardware. Your prompt response would be appreciated. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/8/2016 4:27:11 PMNew subject after splitting |
|
2/7/2016 1:07 AM | |
Joined: 9/27/2006 Last visit: 10/19/2024 Posts: 12289 Rating: (2687) |
Hello Lucky; In the following Application Example, a CPU 317-2DP is programmed with Industry Library v8.0 for integration to a PCS 7 multiproject. I hope this will approximate your situation closely enough. Integration of Comfort Panels, Operator Panels and S7-300 Package Units in SIMATIC PCS 7 with PCS 7 Industry Library https://support.industry.siemens.com/cs/ww/en/view/50708061 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
2/8/2016 10:54 AM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191)
|
Hello,
unfortunately, we don`t have for each possible configuration an example project.
But we have described the most used minimal configurations in the document "PCS 7 Minimal Conficurations:
In your case we have also an application example, it describes how to integrate S7-300 CPUs / Package Units in SIMATIC PCS 7 with PCS 7 Industry Library
|
SIMATIC PCS 7 - Overview |
|
Follow us on