10/23/2019 9:22 AM | |
Joined: 4/19/2015 Last visit: 7/19/2024 Posts: 5 Rating:
|
We use PCS7 V9.0 and will communicate 3 PLC via I-Device. Other PLCs are S7-1500 and S7-300. Other companies generated I-device and gave I-device Gsdml file for profinet. We added gsdml file and it communicated in hardware. We saw communication is OK in HW, this is online and monitoring datas. But in CFC side compile give error. We couldn't fix the error. We finished communication, saw data online in monitoring but how can we fix CFC errors? We are commissioning a Cement Factory and we need a quich solution. Online and error photos in attachment. AttachmentIO_Device_Err.zip (183 Downloads) |
10/23/2019 5:59 PM | |
Joined: 11/29/2011 Last visit: 7/17/2024 Posts: 1358 Rating:
|
Hi, CFC compiler can not recognize you device, so it can not generate Module driver for it. If your IO device is not coming from the SIMATIC Process Control System PCS 7 Released modules (V9.0 SP2) manual, you need to deal with a custom built module driver or will need to compile without "Generate Module Drivers". Further info: |
- What you read here, please check with manuals and your requirements. |
|
Follow us on