12/7/2016 3:27 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, Are the Region and Language settings correctly setup on the client? 1. Make sure all PC stations are equal 2. Set a language which is released for PCS7 such as English (United States), German,French etc. The problem could be that scripts could hang because the system language is not set correctly and the memory goes up. |
If I could help you, you can use the RATE button. Thank you. |
|
9/9/2020 6:26 AM | |
Joined: 8/17/2016 Last visit: 7/14/2022 Posts: 1 Rating: (0) |
Hello, how did your problem end? How was it solved? We now have the same problem on the client |