Industry Online Support
Technical Forum
9/1/2009 11:33 AM | |
Posts: 18 Rating: (0) |
Dear All, Hence the problem needs to be explained with pictures, I have prepared a word document. I will be awaiting for your precious supports. Thanks and Regads... Canan Tas Attachmentos Problem.zip (129 Downloads) |
9/1/2009 12:19 PM | |
Posts: 212 Rating: (12) |
Dear Canan, Please find attached pdf file which is basically talks about HResult Error generated which is shown in one of your snap shot.It talks about 0x80046127 Please try the said solution and revert. Best Wishes. AttachmentV6_0x80046127_e.pdf (134 Downloads) |
9/2/2009 10:47 AM | |
Posts: 18 Rating: (0) |
Dear ABN, The computer name and the login name is the same as before. Attached you can find the screenshots of sql enterprise manager. Attachmentpic.zip (115 Downloads) |
9/2/2009 1:25 PM | |
Posts: 212 Rating: (12) |
Dear canan.tas , you can check one of the options 1. I can see one option now to add one more SQL Server Group via SQL Server Vizard. OR 2.reinstall the machine. OR 3. You can run enableDcom.zip which is attached herewith.also find the information in attached link related to this error. (please read the manual before installing enabledcom.zip) http://support.automation.siemens.com/WW/view/en/6836122 AttachmentEnableDCOM.zip (109 Downloads) |
9/2/2009 1:59 PM | |
Joined: 4/5/2006 Last visit: 10/10/2024 Posts: 917 Rating: (63) |
Hi canan.tas, is it your project WinCC or PCS7? I seen you have WinCCFlexible instance in MSQL, PCS7 and WinCCFlexible have not to be installed on same computer. Regards |
9/2/2009 2:16 PM | |
Joined: 4/5/2006 Last visit: 10/10/2024 Posts: 917 Rating: (63) |
Hi canan.tas , not sure will be enough remove WinCCFlex. I think you can try to remove ALL Siemens Application, then reinstall PCS7. Anyway, what Siemens suggest in this case is a complete reinstallation entire PC (faster if you have original PC image). REgards |
Follow us on