1/25/2014 5:20 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Changing the computer name is not recommended...Officially you have to reinstall windows and pcs7... This is because the SQL databases uses the computer name in his databases and the system could malfunction if you change it... |
Last edited by: Oreca at: 1/25/2014 5:20 PMIf I could help you, you can use the RATE button. Thank you. |
|
2/20/2014 11:01 AM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
That is right. But please notice, the underscore "_" is also an illegal character for computer names since PCS 7 V7.1 SP4! Look at this FAQ. Regards jumo |
Follow us on