4/5/2012 1:07 AM | |
Joined: 11/4/2011 Last visit: 7/22/2024 Posts: 253 Rating:
|
Hello, PCS warriors. Have you ever seen that PH areas won't be accessible in OS Simulation on ES? See attachments: 1. simulation_areas_ru.png ‒ startup language is Russian. When Simulation starts, all area-selection-buttons are blank and Diagnostics button shows <no text>. 2. simulation_areas_en.png ‒ then I change language to English (default language) and Diagnostics button becomes available. 2/3 still missing.. And regardless of step 1 and 2 problems I can go to every picture via Loop in Alarm function of Alarm Window. 3. server_areas_ru/en.png ‒ area buttons are back! (though 'Diagnostics' was at third position earlier.. I don't know..) But also 'Batch name' fields are back (I've hid them) and Russian texts were changed somehow, but this is another story. Advice something about missing area buttons. Many thanks Attachmentattach_AreaButtons.zip (200 Downloads) |
4/23/2012 12:52 PM | |
Joined: 4/20/2010 Last visit: 7/31/2024 Posts: 38 Rating:
|
for preventing trouble because of using different languages here is a document with some good information about that topic and it includes some use case http://support.automation.siemens.com/WW/view/en/56248153 and you are correct the russian package is not availabe for 7.1SP3 strange but I think they want to go to V8. And I'm not sure if i understood your reply, did you made a complete compile and now it works or did you made a complete compile and you have still the same problem? best wishes |
4/27/2012 4:58 PM | |
Joined: 11/4/2011 Last visit: 7/22/2024 Posts: 253 Rating:
|
Hi tomorrow, thank you for reply. I have that document, very useful. Complete compile doesn't help. And the point also is that in Simulation I can switch to English language and see all the areas, then switch back to Russian and still see all the areas right in Russian language. But during start-up the problem still occures. |
Follow us on