2/22/2016 12:06 PM | |
Posts: 29 Rating:
|
Just out of interest - has anyone had a go of PCS7 with Windows 10 yet? I get that it is not officially supported (nor is Win 7 Professional) and as such it would be silly to migrate. I am just wondering if anyone has tried it out ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/23/2016 12:06:00 PMNew subject after splitting |
|
2/25/2016 1:35 PM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating:
|
Windows 10 is not released for PCS 7. In my opinion, it is not necessary, that anybody test it. No customer accepted a software computer constellation, which is not released from Siemens. Why do you want to use Windows 10? |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
1 thankful Users |
8/3/2016 2:13 PM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating:
|
Windows 10 is released with PCS 7 V8.2. Please read the PCS 7 Readme V8.2 to check which station is released, e. g. OS client, BATCH client etc. PCS 7 Readme V8.2: |
Last edited by: Thunderstorm at: 8/4/2016 2:20:59 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to
1 thankful Users |
12/6/2019 6:27 PM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating:
|
Hi, Please be careful with those assumptions! Do you have running PCS7 V9.0 system with Batch control, Route control, using multiple redundant servers and more than one client? And did you test ALL functions of PCS7? Do you have the system running 24/7 for several months? Because that's what Siemens does in Karlsruhe before releasing software. PCS7 could be compatible with the latest update of Windows 10, but Siemens did not release it for a reason. Let's say it works, a new scheduled update is installed, messing up PCS7. Then you're done. That's why the LTSB version is released: Long Time Servicing Branch, making sure no major updates are installed and guarantee a working PCS7 version. The only version released is Windows 10 LTSB 2015 x64 bit Enterprise. Note: LTSB is renamed to LTSC (Long Time Servicing Channel).
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
3 thankful Users |
Follow us on