5/8/2008 4:43 PM | |
Posts: 2661 Rating: (279) |
SKR: Are you familiar with customized objects?If yes, proceed as follows: (If no, read the WinCC manual).
PCS 7 V7.0 Programming Instructions for Blocks http://support.automation.siemens.com/WW/view/en/24449702 Regards |
5/10/2008 7:04 PM | |
Posts: 2661 Rating: (279) |
SKR: I have explained how to create an emf in the attached document. Regards, Phantom AttachmentHow to create a emf.pdf (434 Downloads) |
5/15/2008 9:12 PM | |
Posts: 2661 Rating: (279) |
cabreytj: Thanks for the input. If I remember correctly, with certain combinations of colors and objects the "handles" do get exported. Try the connector object for example. I am not able to recreate this problem but I did face this (probably in older versions). SKR: For exporting symbols from Siemens HMI Library, you drag and drop the symbol to a PDL, adjust the attributes (color, shading etc.)and export to emf. I have attached some sample emf's I exported. Regards Attachmentmot_emf.ZIP (299 Downloads) |
Last edited by: Phantom75 at: 5/15/2008 9:16 PM |
|
5/19/2008 12:21 PM | |
Posts: 13 Rating: (1) |
Dear Phantom Thanx for your response Regards SKR |
Follow us on