12/23/2008 11:04 PM | |
Posts: 9 Rating: (0) |
My HMIversion is V7.5 SP1 - V07.05.01.00 - 5/6/2008 When I DATA IN the PCU 50.3-C says COM active.... then says " Job terminated with error". Under the log is says "the file is not an archive". See the attached .pdf file. AttachmentError Message.pdf (330 Downloads) |
12/24/2008 9:59 AM | |
Joined: 1/29/2008 Last visit: 7/26/2022 Posts: 419 Rating: (19) |
Hello What kind of data do you want to transmit and in which directory? Nit |
12/24/2008 4:35 PM | |
Posts: 9 Rating: (0) |
Part Programs. Below is the header information: %_N_ZN515391OLD_MPF ;$PATH=/_N_MPF_DIR |
12/29/2008 2:13 PM | |
Posts: 9 Rating: (0) |
Karl, Attached is the file. This is the file that was "DATA OUT". I don't see anything wrong. I still think its is a issue with the software or Dino.ini or Dino.exe. Any ideas? AttachmentZN515391.pdf (379 Downloads) |
12/30/2008 9:13 PM | |
Joined: 10/2/2005 Last visit: 9/18/2024 Posts: 32 Rating: (1) |
Try to login with a higher authority level. Maybe with Ev... or Sun... |
12/30/2008 9:22 PM | |
Joined: 10/2/2005 Last visit: 9/18/2024 Posts: 32 Rating: (1) |
Try to remove % after N0580 and make a new DATA IN. |
Follow us on