2/20/2024 5:09 AM | |
Joined: 6/26/2023 Last visit: 3/19/2024 Posts: 4 Rating: (0) |
"I am using TP700 Comfort Panels. For PDF viewing, I can easily read and view 2-3 PDFs, but after some time, the PDFs show a blank screen. I initially thought it was a PDF issue, but the PDFs that were previously viewable are now not displaying. Does anyone have a solution?" i also try factory reset ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/20/2024 07:51:15New subject after splitting |
|
2/20/2024 2:32 PM | |
Joined: 5/6/2022 Last visit: 5/16/2024 Posts: 420 Rating: (83) |
Hi anil02573, In this case, I would recommend two things: - First, check that you have the latest update installed both in the TIA Portal that you are using and in the image version loaded on the TP700 Comfort HMI panel. I don't know the versions you have since you don't indicate them in the post! - On the other hand, I would recommend that you review the following FAQ to see if you meet the requirements and have it configured correctly: "How do you open a Word, Excel or PDF document with a Comfort Panel?" You can also try creating a simple new project by programming the PDF view and see if the same thing happens to you there. The screen may possibly become overloaded. Try what I tell you and if you want, tell us the results! Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on