Industry Online Support
Technical Forum
6/1/2021 1:57 PM | |
Joined: 10/25/2017 Last visit: 7/14/2024 Posts: 5 Rating:
|
Hello, I am trying to configure the project for PDM 9.1 upd 6. I have several CPU 1510SP-1 PN in the PROFINET network, each CPU has several AI modules with HART. I cannot find the CPU 1510SP-1 PN in the PDM object catalog. Automatic search of objects by IP address shows unknown device. For test I tried to add instead of CPU 1510SP-1 PN IM 155-6 PN, diagnosis showed that such a device is and it is GOOD. But in this case, I cannot add AI modules, diagnostics reports "Module not supported." I configured Ai modules as in the ID: 109478959 manual. How do I configure PDM to configure sensors in my system? AttachmentScreens.zip (104 Downloads) |
Follow us on