12/21/2023 8:55 AM | |
Joined: 9/13/2023 Last visit: 7/17/2024 Posts: 13 Rating:
|
Hi, With s7-1500 I have the same problem i can not activate "Permit access with PUT/GET ..." ! Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2023 12:59:22New subject after splitting |
|
This contribution was helpful to
1 thankful Users |
12/21/2023 2:14 PM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating:
|
Hi,
which TIA version is used? If V19 was used, this may be different due to changed security settings. regards sancruz |
Feedback appreciated, please rate |
|
2/26/2024 4:22 AM | |
Joined: 2/7/2021 Last visit: 4/19/2024 Posts: 1 Rating:
|
Hello, good day. Make sure you have a subnet assigned to the port where you will connect your device to the network. You can check this information in the following path: CPU/Properties/Profinet Interface [x-] /Ethernet Address...
|
Follow us on