10/31/2021 4:05 AM | |
Joined: 8/3/2016 Last visit: 4/3/2022 Posts: 2 Rating:
|
Danw, Using the same explanation can i apply it to a DI. In the DI(PB or dry contact ) the Load will be = 24/0.0002. Since the DI is only consuming 2mA. By this logic resistance value comes out to be 12KOhm. Since the input impedance is 3kOhm. So the resistance available for the cable will be 12-3=9 Kohm ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 11/01/2021 14:33:52New subject after splitting |
|
Follow us on