12/25/2023 2:09 PM | |
Joined: 12/6/2023 Last visit: 4/22/2024 Posts: 2 Rating: (0) |
Hi, I need to install PH-ready on Wincc v8.0 redundant servers. The OS on servers is Windows Server 2019. When I start installation from SIMATIC_PH_IS_2020_SP2_Update1 and following steps from manual I get stuck. Problem is when I choose "Process Historian Ready Component 2020" I got message "WinCC Runtime v7.4 SP1 or V7.5 SP1 or V7.5 SP2 or V7.6 is required". Does anyone have solution for this problem? Having regard to this document https://support.industry.siemens.com/cs/cn/en/view/109810551 it shouldn't be a problem with this version of wincc and process historian. |
Last edited by: Jen_Moderator at: 12/27/2023 07:55:36Link optimized. |
|
1/12/2024 2:03 PM | |
Joined: 8/3/2009 Last visit: 5/23/2024 Posts: 12975 Rating: (1653)
|
Hello AutoGen_1412608 in the Compatibility tool you can see that only 2020 SP2 Upd2 is relased with WinCC V8 https://support.industry.siemens.com/cs/ww/en/view/64847781 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on