7/10/2022 11:15 AM | |
Joined: 9/9/2015 Last visit: 5/21/2024 Posts: 727 Rating: (269) |
Hi Berg, Another method for decimal place configuration will be 1. Make use of "Identifier" block attribute. At the function block I/O Properties, configure ##0.000 in your identifier. 2. Then at @PCS7TypicalsAPL.pdl, copy block icon , create another block icons with "AnalogValueformat1" to 4 configured with dynamic ".PV_Out#Value#shortcut" 3. Then compile OS will do. Attached with picture for your reference. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on