Industry Online Support
Technical Forum
12/10/2009 5:58 PM | |
Posts: 27 Rating: (0) |
Greetins Helmut, As always, thanks so much for your answer. I've checked the MW and my current version is V4.0.6.35 I'm using MW SP6. The CPU is a 226 V2.01. Attached you can find my code so you can take a look if you have some time. Sometimes, while the conditions of the PID block are active, the output of this PID block simply don't change. Other solution is to delete the block and drag and drop it again from the subroutines folder in the project tree. After, simply save, compile and download program block again. The problem is this behavior occurs several times while I was with the client and recently occurs two weeks ago and took an entire day to the plan personnel to fix this problem. Any help will be appreciated, thanks for your time. I'll looking forward for your answer. Thanks in advance. Attachment091108 Tipo 2.zip (52 Downloads) |
12/11/2009 9:27 AM | |
Joined: 4/24/2006 Last visit: 6/4/2024 Posts: 8667 Rating: (1154) |
Dear AleksF, I haven't had time to look at programm but I've found the following link: Why does the PID controller created by the instruction wizard sometimes not work? Best regards, Wizard |