1/15/2012 1:24 PM | |
Joined: 7/17/2010 Last visit: 2/17/2024 Posts: 184 Rating: (0) |
Dear colleague I was told to put the call into the OB35 CFs because today I have already in the FB41 FC11 and I wonder if I use the call within the FC11 Ob35 be correct. see the example Attachmentexemp.zip (133 Downloads) |
1/15/2012 7:04 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Dear Martins_Eng, This is what I do suggest to do, call FB41 twice in FC1 and then call FC1 in OB35.See the attachment for more hints! Best regards, Hamid Hosseini AttachmentONE.zip (131 Downloads) |
4/24/2015 9:29 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on