3/29/2018 9:03 AM | |
Joined: 4/28/2015 Last visit: 10/9/2023 Posts: 394 Rating: (55)
|
Hello, the PID control on the S7-1500 is designed as easy-to-use universal PID control and is, because of this, not as flexible as the modular PID control on S7-300. At the moment, the PID control on the S7-1500 is not able to show all MV of P, I and D, only I is possible to see as a separate parameter. For detailed information, please have a look to the manual (https://support.industry.siemens.com/cs/ww/en/view/108210036) or do not hesitate to contact the technical support, for example via Support-Request (https://support.industry.siemens.com/my/ww/en/requests/#createRequest). |
Follow us on