7/27/2015 8:57 PM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating: (1359)
|
Hello chimwana, I would like to find out whether it's possible to implement PID tuning using Particle Swarm Optimization,Model Predictive Control or T-S Fuzzy Logic in S7-300 or S7-400 PLCs?
http://www.amazon.de/Regeln-Mit-SIMATIC-Praxisbuch-Prozessautomatisierung/dp/3895783404 It is possible to test different identification,tuning algorithm and different types of controllers while in a real industrial case, it is preferable to use standard functions developed by manufacturers .If you want to create a function for industry , it should cover wide range of processes, small memory occupation plus fast in execution. I hope this helps, hdhosseini |
Follow us on