4/13/2021 3:44 PM | |
Posts: 3 Rating: (0) |
Hi, I have met the same problem, I would like to ask some questions about this encoder Do you know the Pin definition of P-encode and M-encoder, and also 0V sense and 5V sense(this is the power supply for encoder)? Thanks, best regards.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/14/2021 08:49:15New subject after splitting. Inserted quote. |
|
4/14/2021 8:50 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject The pin defination Encoder I2048 S/R in motor 1FT6105-8SC71 is published within the conference SIMOTICS / MOTION-CONNECT. Jen_Moderator |
Follow us on