10/1/2008 10:05 PM | |
Posts: 7 Rating: (0) |
For WinCC license: 6AV6381-2BC07-0AX0 "WINCC SYSTEMSOFTWARE V7.0, RT 128 (128 POWER TAGS), RUNTIME, ON DVD, SINGLE LICENSE, 5 LANGUAGES (GER,EN,IT,FR,SP), EXEC. UNDER XPPROF/VISTA " Whatexception is in place for XPPROF/VISTA? The five languages? WinCC doc says that XPPROF/VISTA are valid for standalone systems. |
10/1/2008 11:14 PM | |
Posts: 7 Rating: (0) |
The description of the 6AV6381-2BC07-0AX0 license has the text "EXEC. UNDER XPPROF/VISTA" appended to the end. It isunclear whatspecifically is being excepted for XPPROF/VISTA. I understand that WinCC can only be single user for those operating systems, but I do not think the given text is referring to that limitation. |
10/2/2008 5:28 AM | |
Joined: 9/27/2006 Last visit: 1/24/2025 Posts: 12330 Rating: (2702) |
Hello bjc; Youwere provideda very good explanation about the use of the "EXEC." term in the license description above. It means EXECUTABLE. "Executalble under XPprof/vISTA" in this case. Not "exception". Hope this helps, Daniel Chartier |
10/2/2008 7:10 PM | |
Posts: 1275 Rating: (123)
|
Hi, Daniel's right! It means "executable"... as it's been stated, notice that there are different licenses for runtime only and runtime + engineering... and also check compatibility of all Siemens software before purchase... Best regards, Danielle |
Follow us on