10/12/2018 3:47 PM | |
Joined: 4/11/2014 Last visit: 9/1/2021 Posts: 7 Rating: (0) |
Attached another image of the devices and networks since I do not know how to attach several jpg files in the same post |
10/15/2018 12:29 PM | |
Joined: 8/3/2009 Last visit: 12/19/2024 Posts: 14458 Rating: (1806) |
Hello sevekeno You have two situations which you cannot handle in one project: - Runitme on the Panel: here you have a direct communication inside the subnet and this is a normal thing witout problems. - Simulation in your Engineering Station the Engineering PC is in another Subnet. So if you start the simulation the HMI Runtime tries to connect the PLC that is set in the connection in your HMI Project. but this is not possible because its in another Subnet as your Engineering PC. There are scenarios with routing connectinos and so on... but this will only work if you change the connection. so you have to change it every time you want to simulate. So a comfortable way of doing is not possible. But a Project transfer to the HMI with S7-routing is possible (link). Bye Murof |
Last edited by: Murof at: 10/15/2018 12:31:04 PMIf this Information really helps, you could use the Rate function |
|
10/16/2018 7:30 PM | |
Joined: 4/11/2014 Last visit: 9/1/2021 Posts: 7 Rating: (0) |
Thanks for the reply Murof. I understand now that it is not possible. I opened the post because I would swear that at some point I could connect the simulation and see in time the update of the data with the tia portal v13. Now I am working with version 15. The subnet mask on the screen is 255.255.252.0, I understand so that I can connect to the 2 networks .... But with your answers it seems clear that it is not possible to connect online to the screen so I will choose to put a router. Greetings and many thanks! |
This contribution was helpful to1 thankful Users |
10/17/2018 9:55 AM | |
Joined: 8/3/2009 Last visit: 12/19/2024 Posts: 14458 Rating: (1806) |
Thanks for your feedback Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on