Industry Online Support
Technical Forum
11/28/2012 11:05 AM | |
Posts: 10 Rating: (0) |
Hi all, I am trying to connect my with the ET200S but i am failing to do so there is conectivity between the PLC and the PC. I confirmed it with DOS command (ping IP address ) but when i am trying to see the PLC in the sematic manager I am not able to detect my my PLC. One Important thing I am using th VM ware from microsoft in which my semantic is installed.Setting of the VW ware is also attached I have tried to edit the ethernet network node also (tried if see the Mac address for acessible nodesthere just by clicking the browse option ) it does not work also. I am not sure what thing I am doing wrong. I have attaching some snapshots please help me out.. thanks ajai
Attachmentzip.zip (21 Downloads) |
Follow us on