3/4/2024 9:23 AM | |
Joined: 4/8/2022 Last visit: 9/24/2024 Posts: 10 Rating: (0) |
Hi, I have a question in the topic PLC REST Client for MIR Robot REST API. I have been succesfully using the LHTTP Get and Post function blocks for the GET and POST Requests in MIR API. But I couldn't trigger any PUT REQUESTs in the MIR Robot for e.g. I want to pause/play the mission queue of the MIR from the PLC so that an operator doesn't need to use the MIR WebInterface but rather a single process HMI. I am getting error 16#8404, and Response Code 405. Does that meant I can't trigger any PUT requests, and only POST requests can work? Do you have any leads regarding this issue? Thanks in advance! Best regards, Arvind ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/05/2024 08:47:17New subject after splitting |
|
3/4/2024 9:49 AM | |
Joined: 4/8/2022 Last visit: 9/24/2024 Posts: 10 Rating: (0) |
Hi Martin, I am using V2.1.1 |
Follow us on