Industry Online Support
Technical Forum
6/5/2017 8:56 AM | |
Posts: 1 Rating: (0) |
i have to connect 11 S7- 1200 plc with the help of ethernet switch. when i configured in tia portal, i configured only one wincc runtime advance module & plcs , but when i update scada pages and send the pdata file from es to os then one plc data don't came at the time of running of the project. but when i exit the runtime mode minimum 3-4 times then all the plc data will come. so i think its hv some communication problem. so plz help to detect the actual problem . ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/9/2017 4:20:40 PMNew subject after splitting |
|
Follow us on