9/21/2023 2:24 PM | |
Joined: 6/26/2023 Last visit: 7/4/2024 Posts: 21 Rating:
|
Hi Expert, I can ping both from my Laptop. AttachmentPLC_HMI.pdf (322 Downloads) |
9/21/2023 2:48 PM | |
Joined: 5/6/2022 Last visit: 7/16/2024 Posts: 431 Rating:
|
Hi AutoGen_1107196, Firstly, I would like to ask you if both PLC and HMI are simulated, does the communication between them work? I also leave you below some FAQs that can be very helpful in solving these problems: -> Connection configuration: "In WinCC (TIA Portal), how do you configure a connection between WinCC Runtime Advanced or HMI Panel and an S7 controller over Industrial Ethernet (PROFINET)?" -> Possible causes from panel images V17 Update 6: "No connection to PLC after WinCC Panel Images V17 Update 6" I hope they can be of help to you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on