3/10/2013 12:43 PM | |
Posts: 25 Rating: (0) |
Dear All I encountered a problem in S7-416-2DPCPU, that all the LEDs start blinking and PLC goes to inaccessible mode. After restart and download program everything became normal. I want to know the cause, and preventive action to be sure that the problem will not repeat again. Here i attached a diagnostic buffer for reference. Thanks in advance. AttachmentDiagnostic buffer of module CPU 416.pdf (287 Downloads) |
3/10/2013 4:17 PM | |
Joined: 8/25/2005 Last visit: 10/5/2024 Posts: 1162 Rating: (111) |
Hello RahulSharma, there is a newer firmware available. Maybe an update would be helpful? Firmware Updates for S7-416-CPUsIf the CPU is still flashing after the update I would contact the Technical Support Support Request Best regards Sabine |
This contribution was helpful to1 thankful Users |
3/11/2013 10:29 AM | |
Posts: 25 Rating: (0) |
Dear Hulzhex Thanks for reply. Did you find any information from the diagnostic buffer. Thanks |
3/13/2013 3:00 PM | |
Joined: 9/27/2006 Last visit: 11/16/2024 Posts: 12294 Rating: (2691)
|
Hello Rahul; See if the information and the suggested links in the following discussion can help you out: In what case can this all LED flashing occurs if there is a software problem? Hope this helps, Daniel Chartier |
3/14/2013 7:24 AM | |
Posts: 25 Rating: (0) |
Dear dchartier Thanks for the reply, i go through the link given by you. I just want to know that by the diagnostic buffer which i attached is it possible to get a specific reason. Thanks in advance. AttachmentDiagnostic buffer of module CPU 416.pdf (289 Downloads) |
Follow us on